earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: AS-B, IP-IO , MP-C
Funktionaliteter: Maskinvara
Produktversion: 2023, 2024, 7.0
2023-11-30

Output Override Function

arrow1_rotationOverride Display Model for MP-C and IP-IO arrow1_rotationUser Experience arrow1_rotationKeys arrow1_rotationBasic Operation arrow1_rotationOverride Outputs arrow1_rotationView Inputs and Outputs arrow1_rotationConfigure Inputs and Outputs for Temporary Use arrow1_rotationSpecifikationer

The output override function allows you to manually override outputs. This function can be used for testing, commissioning, and maintenance of equipment.

Varning Varning

Unintended equipment operation

Do not override outputs without knowing the effect.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

An override display unit consisting of an LCD display and five keys is provided for override control of the output channels.

 
action_zoom_plus_stroke Override display unit
Figur: Override display unit

The override display also enables you to perform the following actions:

  • View inputs and outputs

  • Configure inputs and outputs

Override Display Model for MP-C and IP-IO

The following override display model is available for use with MP-C controllers and IP-IO modules.

Model

MP-C DISPLAY a

  1. The MP-C DISPLAY model is available in a variant named MP-C-BAA DISPLAY, which is included in Buy American Act (BAA) compliant bundles along with either the MP-C-15A-BAA or MP-C-36A-BAA controller. For more information, see the SpaceLogic MP-C Pro Specification Sheet. MP-C-BAA DISPLAY does not differ from MP-C DISPLAY in terms of hardware and functionality.
Obs!

MP-C controller models with “-M” in the product name do not support the override display unit (MP-C Display).

User Experience

The override display has a menu-driven user interface, which facilitates overriding of the outputs, local configuration of inputs and outputs, and other tasks.

Mer information finns i User Experience .

Keys

You use the keys on the override display to navigate the screens of the user interface and to select options on menus and lists.

Mer information finns i Keys .

Basic Operation

The basic operation of the user interface includes the following actions:

  • Highlight an option on a menu or list

  • Select an option on a menu or list

  • Change a value

Mer information finns i Basic Operation .

Override Outputs

You use the override display to manually override digital outputs as well as analog outputs.

Mer information finns i Override Outputs .

View Inputs and Outputs

Using the override display, you can view the configuration and the present values for inputs and outputs, and for outputs you can also view the override status.

Mer information finns i View Inputs and Outputs .

Configure Inputs and Outputs for Temporary Use

In configuration mode, you can locally configure inputs and outputs for temporary use during commissioning of the device. You can configure inputs and outputs that have not been configured through WorkStation.

Mer information finns i Configure Inputs and Outputs for Temporary Use .

Specifikationer

Display
Display resolution
128 x 64 pixels
Display size
36 W x 17 H mm (1.4 W x 0.7 H in.)
Display type
FSTN monochrome LCD, white color transflective backlight
  • AS-B Servers
  • MP-C Controllers
  • User Experience
  • SpaceLogic MP-C Pro
  • SpaceLogic IP-IO
  • Keys
  • Basic Operation
  • Override Outputs
  • View Inputs and Outputs
  • Configure Inputs and Outputs for Temporary Use