earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: AS-B, IP-IO , MP-C
Функции: Аппаратное обеспечение
Версия продукта: 3.3, 2022, 2023, 2024, 7.0
15.08.2022

User Experience

The override display has a menu-driven user interface, which facilitates overriding of the outputs, local configuration of inputs and outputs, and other tasks.

The main screens of the user interface are briefly described below.

Home screen

The Home screen is displayed when the device is powered on. To go to the next screen, press the Enter key

 
action_zoom_plus_stroke
.

 
action_zoom_plus_stroke Home screen (AS-B server example)
Рисунок: Home screen (AS-B server example)

Более подробную информацию см. Home Screen on AS-B Servers .

Более подробную информацию см. Home Screen on MP-C or IP-IO Module .

I/O Filter screen

The I/O Filter screen provides an overview of the number of I/O points and enables you to filter the I/O List screen on inputs, outputs, and overriden outputs.

 
action_zoom_plus_stroke I/O Filter screen
Рисунок: I/O Filter screen

Более подробную информацию см. I/O Filter Screen .

I/O List screen

The I/O List screen presents the I/O points in a list. You use the screen to view an I/O point, to select an output that you want to override, or to select an I/O point to be locally configured.

 
action_zoom_plus_stroke I/O List screen
Рисунок: I/O List screen

Более подробную информацию см. I/O List Screen .

Output Override screen

The Output Override screen enables you to manually override an output and to remove an override for an output. The screen looks similar for the different types of outputs.

 
action_zoom_plus_stroke  Output Override screen
Рисунок: Output Override screen

Более подробную информацию см. Output Override Screen .

I/O Configuration screen

The I/O Configuration screen is the starting point to locally configure inputs and outputs. To make this screen appear, press and hold down Home key

 
action_zoom_plus_stroke
for three seconds.

 
action_zoom_plus_stroke I/O Configuration screen (AS-B server example)
Рисунок: I/O Configuration screen (AS-B server example)

Более подробную информацию см. I/O Configuration Screen .

  • AS-B Servers
  • MP-C Controllers
  • Output Override Function
  • Home Screen on AS-B Servers
  • Home Screen on MP-C or IP-IO Module
  • I/O Filter Screen
  • I/O List Screen
  • Output Override Screen
  • I/O Configuration Screen
  • Icons
  • Keys