Use the I/O List screen to navigate through the list of I/O points, identify their configuration, view their present values, and identify if an I/O point has a manual override or not.
Component |
Description |
I/O point |
Displays the I/O points in a list. Displays a flashing highlighted I/O point when you are in configuration mode. |
Configuration |
Indicates if and how the I/O point is configured. Более подробную информацию см. Icons . |
Active value |
Displays the present value of the I/O point. |
Manual override |
Indicates if an output has a manual override or not. |
Scroll bar |
Indicates where on the I/O list you are located. |