earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: AS-B, IP-IO , MP-C
Функции: Аппаратное обеспечение
Версия продукта: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
22.07.2021

View Inputs and Outputs

Using the override display, you can view the configuration and the present values for inputs and outputs, and for outputs you can also view the override status.

Icons on the screens indicate the configuration and override status for the inputs and outputs. Более подробную информацию см. Icons .

The value presented for an input or output equals the value transferred in or out to/from the physical device. So even if WorkStation is configured to invert a value from a counter input, digital input, digital output, or digital pulsed output, the override display presents the not inverted value.

 
action_zoom_plus_stroke I/O List screen showing configuration, values, and override status for digital outputs
Рисунок: I/O List screen showing configuration, values, and override status for digital outputs
  • AS-B Servers
  • MP-C Controllers
  • Output Override Function
  • Viewing Inputs and Outputs
  • Icons
  • I/O List Screen