earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, IP-IO , MP-C
Functionalities: Hardware
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
3/13/2019

Viewing Inputs and Outputs

You view inputs and outputs to get information on their configuration or their present values, or to check whether an output is overridden.

Show More
action_close

Using the override display, you can view the configuration and the present values for inputs and outputs, and for outputs you can also view the override status.

Icons on the screens indicate the configuration and override status for the inputs and outputs. For more information, see Icons .

The value presented for an input or output equals the value transferred in or out to/from the physical device. So even if WorkStation is configured to invert a value from a counter input, digital input, digital output, or digital pulsed output, the override display presents the not inverted value.

 
action_zoom_plus_stroke I/O List screen showing configuration, values, and override status for digital outputs
Figure: I/O List screen showing configuration, values, and override status for digital outputs

To view inputs and outputs
  1. With the Home screen displayed, press the Enter key

     
    action_zoom_plus_stroke

  2. Highlight ALL .

     
    action_zoom_plus_stroke
  3. Press the Enter key

     
    action_zoom_plus_stroke
    .

  4. Scroll up/down to the input or output point that you want to view.

     
    action_zoom_plus_stroke
  • View Inputs and Outputs
  • Keys
  • I/O Filter Screen
  • I/O List Screen
  • Icons