earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, IP-IO , MP-C
Functionalities: Hardware
Product version: 3.3, 2022, 2023, 2024, 7.0
7/23/2021

I/O Configuration Screen

Use the I/O Configuration screen to locally configure inputs and outputs, to go to the About screen or Status screen, and to exit the configuration mode.

 
action_zoom_plus_stroke I/O configuration screen
Figure: I/O configuration screen

Table: I/O Configuration Screen

Component

Description

IO Configuration

Select to locally configure inputs and outputs.

About

Select to go to the About screen.

For more information, see About Screen on AS-B Servers .

For more information, see About Screen on MP-C or IP-IO Module .

Status

Select to go to the Status screen (on AS-B servers). For more information, see Status Screen on AS-B Servers .

Exit

Select to exit the configuration mode and return to the Home screen.

  • Configure Inputs and Outputs for Temporary Use
  • About Screen on AS-B Servers
  • About Screen on MP-C or IP-IO Module
  • Status Screen on AS-B Servers
  • Home Screen on AS-B Servers
  • Home Screen on MP-C or IP-IO Module