earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Сигналы тревоги
Версия продукта: 2024, 7.0
02.12.2024

Notification Report Example 2

In the system example, we have created Building A and Building B with a number of identical rooms. We have also created a folder for the repeption area in Building A. In the Reception folder, we have created an analog value and a trend log that logs the temperature in the reception area. The value is connected to an alarm. A notification report that contains the log data is to be displayed in a web browser when a user manually triggers the notification.

We have created a variable triggered notification.

 
action_zoom_plus_stroke Variable triggered notification
Рисунок: Variable triggered notification

We have created a notification report template. The notification report template functions as a template for how notification report content is displayed when the notification is triggered. Более подробную информацию см. Notification Reports .

The template is configured to be displayed as a simple web page that lists the temperature data in an HTML table.

 
action_zoom_plus_stroke The notification report text in HTML including the trend log data
Рисунок: The notification report text in HTML including the trend log data

The trend report data is configured to display each log record as a new table row with two cells: Timestamp and Value.

 
action_zoom_plus_stroke The trend log part of the notification report text in HTML
Рисунок: The trend log part of the notification report text in HTML

We have created a variable triggered notification.

 
action_zoom_plus_stroke Variable triggered notification
Рисунок: Variable triggered notification

The notification is configured to distribute the notification report as a write to file notification with the HTML file extension. The notification report is generated when a user manually triggers the variable triggered notification that uses the notification report template.

 
action_zoom_plus_stroke The file name in the notification specifies the file type that is to be generated
Рисунок: The file name in the notification specifies the file type that is to be generated

The file is accessed from the 'Notification Files' folder of the 'System' folder and is opened in a web browser.

 
action_zoom_plus_stroke The notification report opened in a web browser
Рисунок: The notification report opened in a web browser
  • Notification Reports
  • Notifications
  • Manually Triggering a Notification
  • Notification Report Workflow
  • Notification Report Example 1
  • Creating a Notification Report Template
  • Creating a Variable Triggered Notification