earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WebReports
功能: 报告
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
2021/12/16

Configuring Reports User Account

You use WebReports Administrator to configure the Reports user account and password in Reports Server. Use the same Reports user account and password in the Enterprise Server and the Reports Server to ensure proper communication between the two servers.

显示更多
action_close

WebReports Administrator is a configuration tool to configure the Reports user account in the Reports Server. The user account and password should be same in Enterprise Server and Reports Server to have proper communication between the two servers.

To transfer data from the Enterprise Server to the Reports database, the Reports user account needs to meet the following conditions:

To configure Reports user account
  1. In Windows Explorer, navigate to the folder where the Report Agent is placed. The default folder is C:\Program Files (x86)\Schneider Electric EcoStruxure\Building Operation WebReports\StruxureWare Reporting Agent .

  2. Right-click SE.WebReports.Administrator and then click Run as administrator .

  3. In the User name box, type the name of the Reports user account.

    重要:

    The user account must belong to the Reports Administrators user group. 有关更多信息,请参阅 User Account – Group Membership Tab .

     
    action_zoom_plus_stroke
  4. In the Password box, type the password of the Reports user account.

  5. Click Save .

  • WebReports Administrator - Enterprise Server Configuration
  • WebReports Administrator - Enterprise Server Configuration Dialog Box
  • User Account – Group Membership Tab
  • Could not Connect to Reports Database
  • Authentication Failed