earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2023
2022/12/16

Create Alarm Decoration Rule Wizard - User Action Page

Use the User Action page or tab configure the user action required when the alarm decoration rule conditions are met.

 
action_zoom_plus_stroke User Action page
图: User Action page

表格: User Action Page or Tab

Property

Description

Override

Select the boxes for the user action properties you want to override when the alarm decoration rule conditions are met.

Cause note group

Enter the cause note group that is used by the alarm when the alarm decoration rule conditions are met.

有关更多信息,请参阅 User Actions .

Action note group

Enter the action note group that is used by the alarm when the alarm decoration rule conditions are met.

有关更多信息,请参阅 User Actions .

Checklist

Enter the checklist that belongs to the alarm when the alarm decoration rule conditions are met.

有关更多信息,请参阅 User Actions .

Required User Actions

Select what actions the user has to perform when any of the listed events occur and when the alarm decoration rule conditions are met.

有关更多信息,请参阅 User Actions .

  • Alarm Decoration
  • User Actions
  • Create Object Dialog – Naming the Object Page
  • Create Alarm Decoration Rule Wizard - Filter Page
  • Create Alarm Decoration Rule Wizard - Presentation Page
  • Create Alarm Wizard – Attachment Page