earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2023
2022/12/16

Create Alarm Decoration Rule Wizard - Filter Page

Use the Filter page or tab to configure the conditions that have to be met before the alarm decoration rule overrides the original properties configured for the alarm.

 
action_zoom_plus_stroke Filter page
图: Filter page

表格: Filter Page or Tab

Property

Description

 
action_zoom_plus_stroke

Add condition

Click to add the conditions that have to be met before the alarm decoration rule becomes active and overrides the original configuration of the alarm. 有关更多信息,请参阅 添加/移除条件对话框 .

 
action_zoom_plus_stroke

Remove condition

Click to remove the selected condition.

 
action_zoom_plus_stroke

Add row

Click to add another condition that has to be met before the alarm decoration rule becomes active.

 
action_zoom_plus_stroke

Remove row

Click to remove the selected alarm decoration rule condition.

Clear all

Click to clear the selected conditions.

  • Alarm Decoration
  • 添加/移除条件对话框
  • Alarm Filters
  • Create Object Dialog – Naming the Object Page
  • Create Alarm Decoration Rule Wizard - Presentation Page
  • Create Alarm Decoration Rule Wizard - User Action Page
  • Create Alarm Wizard – Attachment Page