earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmas
Versión del producto: 3.2, 3.3, 2022
15/10/2020

Create Alarm Decoration Rule Wizard - Filter Page

Use the Filter page or tab to configure the conditions that have to be met before the alarm decoration rule overrides the original properties configured for the alarm.

 
action_zoom_plus_stroke Filter page
Figura: Filter page

Tabla: Filter Page or Tab

Property

Description

 
action_zoom_plus_stroke

Add condition

Click to add the conditions that have to be met before the alarm decoration rule becomes active and overrides the original configuration of the alarm. Para obtener más información, consulte Add/Remove Conditions Dialog Box .

 
action_zoom_plus_stroke

Remove condition

Click to remove the selected condition.

 
action_zoom_plus_stroke

Add row

Click to add another condition that has to be met before the alarm decoration rule becomes active.

 
action_zoom_plus_stroke

Remove row

Click to remove the selected alarm decoration rule condition.

Clear all

Click to clear the selected conditions.

  • Alarm Decoration
  • Add/Remove Conditions Dialog Box
  • Alarm Filters
  • Create Object Dialog – Naming the Object Page
  • Create Alarm Decoration Rule Wizard - Presentation Page
  • Create Alarm Decoration Rule Wizard - User Action Page
  • Create Alarm Wizard – Attachment Page