earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface utilisateur

Interface utilisateur


Produits : AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Alarmes
Version produit : 2.0, 2.1, 3.0, 3.1
18/12/2018

Create Alarm Decoration Rule Wizard - Filter Page

Use the Filter page or tab to configure the conditions that have to be met before the alarm decoration rule overrides the original properties configured for the alarm.

 
action_zoom_plus_stroke Filter page
Figure : Filter page

Table : Filter Page or Tab

Property

Description

 
action_zoom_plus_stroke

Add condition

Click to add the conditions that have to be met before the alarm decoration rule becomes active and overrides the original configuration of the alarm. Pour plus d'informations, voir Boîte de dialogue Ajouter/Supprimer des conditions .

 
action_zoom_plus_stroke

Remove condition

Click to remove the selected condition.

 
action_zoom_plus_stroke

Add row

Click to add another condition that has to be met before the alarm decoration rule becomes active.

 
action_zoom_plus_stroke

Remove row

Click to remove the selected alarm decoration rule condition.

Clear all

Click to clear the selected conditions.

  • Alarm Decoration
  • Boîte de dialogue Ajouter/Supprimer des conditions
  • Alarm Filters
  • Create Object Wizard – Naming the Object Page
  • Create Alarm Decoration Rule Wizard - Presentation Page
  • Create Alarm Decoration Rule Wizard - User Action Page
  • Create Alarm Wizard – Attachment Page