earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 2.0, 2.1, 3.0, 3.1
18/05/2018

Mass Renaming Objects 

You mass rename objects to make renaming more efficient and consistent.

Afficher plus
action_close

Use mass edit when you want to change several property values or rename several objects at a time.

You can change several property values at a time, for example, when you want to change all setpoints from 22 to 20. Pour plus d'informations, voir Mass Editing Objects .

 
action_zoom_plus_stroke Multi editing
Figure : Multi editing

The objects do not need to be of the same type to be mass edited. However, the properties you want to edit have to be of the same type.

You can mass rename all objects that are possible to move. For example, you can rename alarms but not properties.

You can rename the objects one by one. You can also copy row-separated text from a file, such as an MS Excel file, and paste it to rename several rows in one single operation. When you paste, the copied text is pasted from the row you have clicked and down in the list. If the copied text is longer than the number of rows, pasting stops at the last row.

Pour plus d'informations, voir Mass Renaming Objects  .

Pour plus d'informations, voir Mass Renaming Objects Using Copy and Paste  .

When you hover over the names in the Name column, the full path of the object is displayed.

You can mass change the units of objects in a search result. Pour plus d'informations, voir Mass Changing Units .

To mass rename objects
  1. In WorkStation, select the container for the objects you want to rename or perform a search.

  2. In the List View or Search View , select the objects you want to rename.

  3. On the Edit menu, click Rename .

  4. In the Rename dialog box, in the New name column, select the object name you want to change and type or paste the new name.

  5. Click OK .

  • Mass Edit
  • Vue Liste
  • Search View
  • Moving Objects
  • Mass Renaming Objects Using Copy and Paste