earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Trends
Product version: 2023
12/17/2022

Manually Adding a Trend Log Record to a Trend Log List

You manually add trend log records if a log record has been missed and you want to complete the list or to add old values to compare the log record history to.

Show More
action_close

A trend log list displays all values in the trend log in a list.

You can create a trend log list directly from a trend log and refresh the values.

You can manually add records to a trend log list for any type of trend log.

Trend Log List Display

A trend log list can be displayed in a number of ways.

For more information, see Trend Log List Display .

Export of Trend Log Lists and Records

Trend log lists and records can be exported in two different formats:

  • CSV

  • XML

For more information, see Export of Trend Log Lists and Records .

 
action_zoom_plus_stroke Trend log list
Figure: Trend log list

To manually add a trend log record to a trend log list
  1. In WorkStation, in the System Tree pane, select the folder or EcoStruxure BMS server where the trend log list is located.

  2. Select the trend log list to which you want add a record.

  3. On the trend log list toolbar, click Add trend log record

     
    action_zoom_plus_stroke
    .

  4. In the Add trend log record dialog box, in the Time stamp box, enter the date and time of the new value.

  5. In the Value box, enter the value.

  6. In the Comment box, type a comment.

  7. Click Add record .

  8. Click Close .

The record is now added to the trend log list.

  • Trend Log Lists in WorkStation
  • Add Trend Log Record Dialog Box
  • Trend Log Lists
  • Editing or Commenting a Trend Log Record
  • Manually Adding a Trend Log Record to a Trend Log