earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AD v2
功能: 硬件
产品版本: 1.8, 1.9
2017/6/16

Installing the AD v2 Tablet and Frame

You install the AD v2 tablet and the frame on the base to install AD v2 on a control cabinet or a wall and to provide the tablet with a protective frame.

显示更多
action_close

AD v2 is the successor to AD v1, and offers several improvements such as higher display resolution, enhanced processor performance, and increased memory size. Like AD v1, AD v2 provides a Human Machine Interface (HMI) for local access to SmartStruxure servers.

AD v2 is based on an Android platform with a high-resolution touchscreen display. The display size is 10.1 inches.

 
action_zoom_plus_stroke AD v2
图: AD v2

AD v2

AD v2 is intended to be used as a stationary HMI terminal. For example, AD v2 can be installed on a control cabinet in a plant room or it can be installed on a wall in a hospital.

Kiosk Mode

AD v2 is preinstalled with SmartXKiosk, which allows you to lock AD v2 into Kiosk mode to prevent users from accessing other apps than the one you have downloaded and selected. 有关更多信息,请参阅 SmartXKiosk Overview .

AD v2 Bundle

AD v2 is delivered in a bundle, which contains a protective frame. When assembled, the frame protects against dust, moisture, and mechanical damage. The USB cable is ordered separately from Schneider Electric.

注释:

The frame and its base do not provide protection against theft.

Installation Options

The protective frame has a base, which is equipped with hole mount patterns to support a variety of installation options. For example, AD v2 can be installed on a control cabinet, on a wall, or on a VESA stand that fits devices with a 100 x 100 mm (3.94 x 3.94 in.) hole pattern.

AD v2 Communication and Power

AD v2 can use either a wired (USB) connection or a wireless (WiFi) connection to communicate with SmartStruxure servers. AD v2 can be powered either by an AS-P, AS-B, or USB power adapter, but not by an Automation Server.

有关更多信息,请参阅 AD v2 Communication and Power .

Preinstalled Apps

AD v2 is delivered with the following set of preinstalled apps:

  • SmartXKiosk for locking AD v2 into Kiosk mode

  • SmartX AD-Link for enabling IP over USB communication

    有关更多信息,请参阅 SmartX AD-Link Overview .

  • Technician Tool for operation and maintenance of SmartStruxure servers

    有关更多信息,请参阅 技术人员工具概览 .

  • AdaptiApps shell apps for deployment of AdaptiApps end user apps

规格

Electrical
DC input current consumption
500 mA to 1.3 A
DC input supply voltage
5 VDC (USB)
Environment
Ambient temperature, operating
5 to 35 °C (41 to 95 °F)
Ambient temperature, storage
-20 °C to +60 °C (-4 °F to +140 °F)
Maximum humidity
95 % RH non-condensing
Material
Enclosure
UV stable ABS
Enclosure rating
IP 54
Plastic rating
UL94-HB
Mechanical
Dimensions (W x H x D)
301 x 167 x 19 mm (11.8 x 6.6 x 0.75 in.)
 
action_zoom_plus_stroke
Weight
0.743 kg (1.638 lb)
Communications
USB
1 USB 2.0 port
WiFi
802.11 a/b/g/n/ac 2.4 + 5 GHz, VHT80
CPU
Frequency
1.6 GHz
Type
Octa-core (8-core)
Internal memory
2 GB RAM, 16 GB ROM
Operating system
Supported versions
Android 6.0 (Marshmallow)
Display
Display resolution
1,920 x 1,200 pixels
Display aspect ratio
16:10
Display size
10.1 inches (255 mm)
Display type
TFT LCD, touchscreen

To install the AD v2 tablet and frame
  1. Thread the USB cable through the hole in the cabinet or wall and through the center hole (cable grommet) in the base.

  2. Route the cable from the center hole to the left side of the base.

     
    action_zoom_plus_stroke
  3. Carefully insert the tablet into the base from above and then slide the tablet completely into the base.

     
    action_zoom_plus_stroke
  4. Insert the USB cable into the tablet's charger/accessory port.

    通知

    数据丢失

    Use only USB cables ordered from Schneider Electric. Using a cable that exceeds 3 m (10 ft) or that is not designed for AD can cause loss of data or power.

    不遵照这些说明可导致数据丢失。

     
    action_zoom_plus_stroke
  5. Fit the ribs inside the top of the frame to the base and hook the frame onto the base.

  6. Push the frame onto the base.

  7. Fit the security screws (M4 x 0.7 x 10 mm) to the screw inserts at the bottom of the frame and tighten the screws using a T20 Security TORX screwdriver or bit.

     
    action_zoom_plus_stroke

You can now make the required connections for power supply and communication with the SmartStruxure servers.

  • AD v2
  • Installing the AD v2 Base on a Cabinet
  • Installing the AD v2 Base on a Wall
  • Connecting AD to a Power Adapter
  • Connecting AD to AS-P or AS-B
  • Connecting AD to Automation Server and a Power Adapter
  • AD Does Not Turn On or Battery Does Not Charge