earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: User Management
Product version: 2023
12/17/2022

Workspace Path, Object, and Command Customization

Software permissions limit the paths, objects, and commands that are available in a workspace. For example, a user with No Access permissions for a particular path cannot see any of the path objects displayed in the System Tree pane. A user with Read permissions for a path can see the path objects but cannot issue any commands because the objects are not made available.

For more information, see Software Permissions .

Workspaces and software permissions are linked to user account groups. User accounts inherit the workspaces and permissions of all user account groups in which the user account is a member. For more information, see Software Permissions, User Accounts, and User Account Groups .

  • Workspace Customization
  • Workspace Components and Customization
  • Software Permissions
  • Software Permissions, User Accounts, and User Account Groups