Funzionalità: Allarmi
Versione del prodotto: 2023
17/12/2022

Custom Audible Alarm Alert Workflow

A custom audible alarm alert is an audio file that is played when an alarm is triggered.

 
action_zoom_plus_stroke Custom audible alarm alert flowchart
Figura: Custom audible alarm alert flowchart
Add an Audio File for a Custom Audible Alarm Alert

Add the custom audio file to the EcoStruxure BMS server where you want to hear the custom audible alarm alert.

Per maggior informazioni, consulta Adding an Audio File for a Custom Audible Alarm Alert .

Configure a Custom Audible Alarm Alert

Configure the alarm to play the custom audio file when the alarm is triggered or reset.

Per maggior informazioni, consulta Configuring a Custom Audible Alarm Alert .

  • Custom Audible Alarm Alerts
  • Alarm Functions
  • Adding an Audio File for a Custom Audible Alarm Alert
  • Configuring a Custom Audible Alarm Alert