Backup sets are stored in different locations for stand-alone systems and multi-server systems.
In a multi-server system with an Enterprise Server and one or more SmartX servers, the backup sets are stored on the computer that runs the Enterprise server. The SmartX server also store its own backup set.
In a multi-server system with an Enterprise Central and one or more attached Enterprise Servers, the backup sets for the Enterprise Central are stored on the computer running the Enterprise Central. The backup sets for the attached Enterprise Servers are stored on the computers running the Enterprise Servers.
Using WorkStation, you can copy the backup set to a location other than the EcoStruxure BMS server.
Pour plus d'informations, voir Copying a Backup Set to the Enterprise Server or Enterprise Central Local Directory .
In the Backup sets folder of the installation directory, two directories are created:
AS Archives : Lists separate subfolders that reflect the name of each SmartX server. Each subfolder contains the backup files for that SmartX server.
Local : Lists all the local backup files for the Enterprise Server and Enterprise Central.
In a stand-alone system the backup set is saved in the Smart Struxure server device. Using WorkStation, you can save the backup set to a location other than the SmartX server.
Pour plus d'informations, voir Saving a SmartX Server Backup Set to Another Location .
The SmartX server stores only one backup set at a time, so each new backup operation overwrites the previous backup set.