The MP-V models offer a versatile mix of I/O point types that match a wide variety of VAV applications.
I/O Point Types |
MP-V-7A |
MP-V-9A |
Universal inputs |
3 |
4 |
Triac outputs |
3 |
3 |
Analog outputs |
1 |
2 |
The universal inputs are ideal for any mix of temperature, pressure, flow, status points, and similar point types in a building control system.
Więcej informacji zawiera Universal Inputs .
The triac outputs can be used in many applications to switch 24 VAC on or off for external loads such as actuators, relays, or indicators. Triacs are silent and do not suffer from relay contact wear.
Więcej informacji zawiera Triac Outputs .
The analog outputs are capable of supporting analog voltage or current point types. Therefore, analog outputs support a wide range of devices, such as actuators.
Więcej informacji zawiera Analog Outputs .