earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Alarms
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
5/18/2018

Adding a Comment to an Alarm in WebStation

You add a comment to an alarm to help others understand the problem that caused the alarm or how the alarm was solved.

Show More
action_close

You can add a comment to an alarm that can be helpful the next time the same alarm is triggered.

Other people can read your comment in WorkStation or WebStation. You can add a comment to an alarm that is assigned to yourself or to someone else.

Your comment is marked with your user name and the time you made the comment.

In some cases, adding a comment to an alarm is optional. In other cases, you are required to add a comment when you acknowledge the alarm.

You add a comment using WorkStation or WebStation. You can view a comment added to an alarm in WorkStation and WebStation.

To add a comment to an alarm in WebStation
  1. In the Alarms pane, click the alarm.

  2. In the Alarm Details dialog box, click Comments

  3. In the Add Comment dialog box, type the comment.

  4. Click Send .

  5. Click Close .

  • Alarm Comments
  • Comment Dialog Box
  • Alarm Details Dialog Box