earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Basic Functionality
Product version: 2022, 2023, 2024
7/5/2022

Settings Menu – Options Tab

Use the Settings menu to select workspace, change password, change regional settings, add or remove languages, or log off.

 
action_zoom_plus_stroke Options tab
Figure: Options tab

Table: Options Tab

Command

Description

Change password

Click to open the Change password dialog box where you change your password. For more information, see Change Password Dialog Box .

User settings

Click to open the user settings Regional Settings and Theme Settings menus.

For more information, see User Settings – Regional Settings Dialog Box . 

For more information, see User Settings – Theme Settings Tab .

Settings

Click to open the default system Settings menu.

Add or remove language

Click to open the Add or remove language dialog box where you add or remove languages. For more information, see Add or Remove Languages Dialog Box .

Preview features

Click to open the Preview features menu.

About WebStation

Click to view the version of WebStation you are using.

Log off

Click to log off.

  • Workspaces
  • Change Password Dialog Box
  • User Settings – Regional Settings Dialog Box
  • User Settings – Theme Settings Tab
  • Settings – Default Regional Settings Dialog Box
  • Default System Settings – Theme Settings Tab
  • Language Packages
  • Regional Settings
  • Add or Remove Languages Dialog Box