Produkty: WebStation
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 2022, 2023
2022-07-05

Settings Menu – Options Tab

Use the Settings menu to select workspace, change password, change regional settings, add or remove languages, or log off.

 
action_zoom_plus_stroke Options tab
Rysunek: Options tab

Tabela: Options Tab

Command

Description

Change password

Click to open the Change password dialog box where you change your password. Więcej informacji zawiera Change Password Dialog Box .

User settings

Click to open the user settings Regional Settings and Theme Settings menus.

Więcej informacji zawiera User Settings – Regional Settings Dialog Box . 

Więcej informacji zawiera User Settings – Theme Settings Tab .

Settings

Click to open the default system Settings menu.

Add or remove language

Click to open the Add or remove language dialog box where you add or remove languages. Więcej informacji zawiera Add or Remove Languages Dialog Box .

Preview features

Click to open the Preview features menu.

About WebStation

Click to view the version of WebStation you are using.

Log off

Click to log off.

  • Workspaces
  • Change Password Dialog Box
  • User Settings – Regional Settings Dialog Box
  • User Settings – Theme Settings Tab
  • Settings – Default Regional Settings Dialog Box
  • Default System Settings – Theme Settings Tab
  • Language Packages
  • Regional Settings
  • Add or Remove Languages Dialog Box