Use the Right axis tab in WebStation to change the settings for the right axis of a trend chart.
Component |
Description |
Show gridlines for right Y-axis |
Select True to show grid lines originating from the right y-axis scale. For more information, see Showing Trend Chart Grid Lines . |
Right scale |
Select if you want to display the axis linear or logarithmic. |
Auto scale right Y-axis |
Select True to activate auto scale. The scale of the right axis automatically adapts to the displayed series. For more information, see Automatically Configuring the Y-axis Scale . Clear to deactivate auto scale. Manually scale the left axis by typing values in the Right Y-axis minimum and Right Y-axis maximum boxes |
Right Y-axis minimum |
Type the minimum value of the right y-axis. For more information, see Manually Configuring the Y-Axis Scale . |
Right Y-axis maximum |
Type the maximum value of the right y-axis. For more information, see Manually Configuring the Y-Axis Scale . |