earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Trends
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
5/18/2018

Trend Chart Settings Dialog Box – Right Axis Tab

Use the Right axis tab in WebStation to change the settings for the right axis of a trend chart.

 
action_zoom_plus_stroke Right axis tab
Figure: Right axis tab

Table: Right Axis Tab

Component

Description

Show gridlines for right Y-axis

Select True to show grid lines originating from the right y-axis scale.  For more information, see Showing Trend Chart Grid Lines .

Auto scale right Y-axis 

Select True to activate auto scale. The scale of the right axis automatically adapts to the displayed series. For more information, see Automatically Configuring the Y-axis Scale .

Clear to deactivate auto scale. Manually scale the left axis by typing values in the Right Y-axis minimum and Right Y-axis maximum boxes

Right Y-axis minimum 

Type the minimum value of the right y-axis. For more information, see Manually Configuring the Y-Axis Scale .

Right Y-axis maximum

Type the maximum value of the right y-axis. For more information, see Manually Configuring the Y-Axis Scale .

  • Trend Chart Series in WebStation
  • Trend Series
  • Trend Chart Series Menu
  • Trend Chart Settings Dialog Box – X Axis Tab
  • Trend Chart Settings Dialog Box – Series Tab