Use this workflow with the eCommission SmartX Controllers mobile application to check out I/O following the installation and wiring of MP Series controllers and other devices. Complete the tasks listed in the following flowchart. Information related to each task can be found in the sections following the flowchart.
Physically wire together the MP Series controllers and other devices that are to be connected.
Connect the eCommission application to the MP Series controllers.
For more information, see Connection and Architecture Options .
Start the eCommission application and log in, and then discover MP Series controllers on the network.
For more information, see Downloading and Starting the eCommission SmartX Controllers Mobile Application .
For each MP Series controller, perform checkout of its inputs and outputs.
For more information, see Performing I/O Checkout .
After connecting and checking out the MP Series controllers, you can proceed to other tasks as needed:
Capture device information from the controllers
For more information, see Capturing a Device with the Controller List Creator .