earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
2
Concept

Concept


Products: Commission, IP-IO , MP-C, MP-V, RP-C
Functionalities: Engineering, BACnet/IP devices
Product version: 3.0, 3.1, 3.2
7/13/2019

eCommission SmartX Controllers Mobile Application Overview

arrow1_rotationPreparations arrow1_rotationDevice Connection arrow1_rotationBluetooth Adapter arrow1_rotationDevice Settings arrow1_rotationImage Downloading arrow1_rotationConfiguration Menu arrow1_rotationI/O Checkout arrow1_rotationFlow Balancing arrow1_rotationDevice Restart

The eCommission SmartX Controllers mobile application allows you to use a mobile device to perform commissioning, flow balance, and checkout operations on SmartX IP controllers. SmartX IP controllers include MP and RP Series controllers and IP-IO devices. The eCommission application is available for Android and iOS (Apple) phones and tablets, as well as devices using Microsoft Windows 10. The eCommission app can connect to a single SmartX IP controller or to a network of SmartX IP controllers on the local network.

Preparations

Prior to using the eCommission SmartX Controllers mobile application at a job site, there are some preparations you must make to facilitate device commissioning.

For more information, see Preparations .

Device Connection

The eCommission SmartX Controllers application supports device connection through BACnet Wi-Fi and wireless Bluetooth connection.

For more information, see Device Connection .

Bluetooth Adapter

The eCommission Bluetooth Adapter allows you to establish a Bluetooth connection to MP Series controllers. You plug the Bluetooth Adapter into the corresponding SmartX Sensor to connect to the controller.

For more information, see eCommission Bluetooth Adapter .

Device Settings

The Device Settings view of the eCommission SmartX Controllers mobile application allows you to configure most of the settings of the SmartX IP controller. You can save a particular device settings configuration to a Common Settings file. Common Device Settings files can be downloaded to multiple SmartX IP controllers to facilitate device configuration.

For more information, see SmartX IP Controller Device Settings .

Image Downloading

Image files are created by a WorkStation user and contain pre-engineered objects, properties, and values. Download an Image to a SmartX IP controller to facilitate device commissioning tasks.

For more information, see Image Downloading .

Configuration Menu

Configuration Menus are a group of pre-engineered objects and values that make device commissioning faster and easier. Configuration Menus are exported and downloaded from image files. Download a Configuration Menu to a SmartX IP Controller to commission the controller.

For more information, see Configuration Menu .

I/O Checkout

After you have wired the physical inputs and outputs of the controller, you perform I/O checkout to verify that the wiring was done correctly and that the physical inputs and outputs are working properly.

For more information, see I/O Checkout Overview .

Flow Balancing

The Flow Balance function of the eCommission SmartX Controllers mobile application is used to air balance terminal boxes controlled by MP-V controllers. This function automates most of the air balance procedure but it also allows you to manually check out the flow balance by driving the damper to a specified position, a flow setpoint, or a flow value.

For more information, see Flow Balancing .

Device Restart

Use the Device Restart function of the eCommission SmartX Controllers application to perform a restart of the SmartX IP controller. There are four different ways to restart the SmartX IP controller.

For more information, see Device Restart .

  • Preparations
  • Device Connection
  • eCommission Bluetooth Adapter
  • SmartX IP Controller Device Settings
  • Image Downloading
  • Configuration Menu
  • I/O Checkout Overview
  • Flow Balancing
  • Device Restart