Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
The eCommission SmartX Controllers mobile application allows you to use a mobile device to perform commissioning, flow balance, and checkout operations on SpaceLogic BACnet/IP devices. BACnet/IP devices include BACnet/IP controllers (MP and RP) and IP-IO modules. The eCommission application is available for Android and iOS (Apple) phones and tablets, as well as devices using Microsoft Windows 10. The eCommission app can connect to a single BACnet/IP device or to a network of BACnet/IP devices on the local network.
Prior to using the eCommission SmartX Controllers mobile application at a job site, there are some preparations you must make to facilitate device commissioning.
For more information, see Preparations .
The eCommission SmartX Controllers application supports device connection through BACnet Wi-Fi and wireless Bluetooth connection.
For more information, see Device Connection .
The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to MP controllers. You plug the Bluetooth Adapter into the corresponding SpaceLogic Sensor to connect to the controller.
For more information, see SpaceLogic Bluetooth Adapter .
The Device Settings view of the eCommission SmartX Controllers mobile application allows you to configure most of the settings of the BACnet/IP controller. You can save a particular device settings configuration to a Common Settings file. Common Device Settings files can be downloaded to multiple BACnet/IP controllers to facilitate device configuration.
For more information, see BACnet/IP Controller Device Settings .
Image files are created by a WorkStation user and contain pre-engineered objects, properties, and values. Download an Image to a BACnet/IP controller to facilitate device commissioning tasks.
For more information, see Image Downloading .
Configuration Menus are a group of pre-engineered objects and values that make device commissioning faster and easier. Configuration Menus are exported and downloaded from image files. Download a Configuration Menu to a BACnet/IP controller to commission the controller.
For more information, see Configuration Menu .
After you have wired the physical inputs and outputs of the controller, you perform I/O checkout to verify that the wiring was done correctly and that the physical inputs and outputs are working properly.
For more information, see I/O Checkout Overview .
The Flow Balance function of the eCommission SmartX Controllers mobile application is used to air balance terminal boxes controlled by MP-V controllers. This function automates most of the air balance procedure but it also allows you to manually check out the flow balance by driving the damper to a specified position, a flow setpoint, or a flow value.
For more information, see Flow Balancing .
Use the Device Restart function of the eCommission SmartX Controllers application to perform a restart of the BACnet/IP controller. There are four different ways to restart the BACnet/IP controller.
For more information, see Device Restart .