Commission 移动应用是用于在 SpaceLogic BACnet/IP 设备上执行调试、风量平衡和检出操作的专用移动应用。BACnet/IP 设备包括 BACnet/IP-控制器(MP 和 RP)和 IP-IO 模块。Commission 应用程序适用于 Android 和 iOS (Apple) 手机和平板电脑,以及使用 Microsoft Windows 10 的设备。Commission 移动应用程序可以连接到单个 BACnet/IP 设备或本地网络上的 BACnet/IP 设备网络。
The Commission mobile application supports device connection through BACnet Wi-Fi and wireless Bluetooth connection.
有关更多信息,请参阅 设备连接 .
The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to SpaceLogic and EasyLogic controllers that contain an extra COM port. You plug the Bluetooth adapter into the corresponding SpaceLogic Sensor to connect to the controller.
有关更多信息,请参阅 SpaceLogic 蓝牙适配器 .
You configure the device settings of a BACnet/IP device so that it can communicate on the network. For example, in the Commission Mobile Application, you can configure the BACnet/IP controller so that it can communicate on the IP network, or configure it as an MS/TP device to enable it to communicate on an MS/TP network.
有关更多信息,请参阅 BACnet/IP 控制器设备设置 .
Configuration Menus are a group of pre-engineered objects and values that make device commissioning faster and easier. Configuration Menus are exported and downloaded from image files. Download a Configuration Menu to a BACnet/IP controller to commission the controller.
有关更多信息,请参阅 配置菜单 .
After you have wired the physical inputs and outputs of the controller, you perform I/O checkout to verify that the wiring was done correctly and that the physical inputs and outputs are working properly.
有关更多信息,请参阅 I/O 检出概览 .
The Flow Balance function of the Commission mobile application is used to air balance terminal boxes controlled by VAV controllers. This function automates most of the air balance procedure but it also allows you to manually check out the flow balance by driving the damper to a specified position, a flow setpoint, or a flow value.
有关更多信息,请参阅 风量平衡 .
Use the Device Restart function of the Commission mobile application to perform a restart of the BACnet/IP controller. There are four different ways to restart the BACnet/IP controller.
有关更多信息,请参阅 设备重启 .