The Commission mobile application provides the user with a means to generate a flow balance report that documents several values:
Box capacity at 1 inch H 2 O (249 Pa)
Box measured flow
Hood measured flow for each setpoint used during balancing
Actuator stroke and rotation
Flow balance time and date
Any comments
Using the Commission mobile application, you can create, append, and delete flow balance reports. Flow balance reports are stored on the Commission mobile application mobile device and can be retrieved and shared using the file and e-mail applications of that mobile device or Windows laptop.
After flow balancing a VAV unit, you can use the Commission mobile application to create a new flow balance report, append an existing flow balance report with new information, view an existing flow balance report, or delete flow balance reports that are no longer needed.
After flow balancing a VAV unit, you can use the Commission mobile application to create, append, view, or delete flow balance reports.
For more information, see Managing Flow Balance Reports .
The flow balance report file is stored on your phone or laptop in the CommissioningTool\ FlowBalanceReport folder. You can navigate to this folder, using either of two methods:
You can use a file navigation utility on the mobile device, for example File Explorer (Windows devices), to perform a search for the folder name.
You can select and copy all the contents of the Location box and then paste the text into the search box of a file navigation utility on the mobile device, for example File Explorer, and then execute the search.
File organization, and navigation within the file structure, varies from one Android platform to another. Therefore, you may need to try more than one approach when searching for the flow balance report file.
Once you have located the report file, it can be exported. Alternatively, you can share the report directly from the Commissioning mobile application.