After flow balancing a VAV unit, you can use the eCommission SmartX Controllers mobile application to create, append, view, or delete flow balance reports.
In the Flow balance function, on the Air Balancing menu, select Balance report .
In the Balance Report view, in the Device List , select the check boxes to select the MP-V controllers you want to include in the report. If you wish to include all the listed controllers in the report, select Select all .
Select Create .
In the Create dialog box, in the Report name box, type the report name.
In the Project name box, type the project name.
In the Engineer box, type the engineer name.
In the Create dialog box, the Location box contains the directory path where the flow balance report file is located. If you will export the report file later, copy the directory path to the clipboard. To do this, select the path in the Location box, choose Select All , and then select Copy .
Select OK to create the flow balance report file.
Once the flow balance report file is created, it can be exported. Find the report file by navigating to the CommissioningTool\ FlowBalanceReport folder, using either of two methods:
You can use a file navigation utility on the mobile device, for example File Explorer (Windows devices), to perform a search for the folder name.
You can follow the path you previously saved to the clipboard. To do this, start a file navigation utility on the mobile device, for example File Explorer, paste the path text into the search box, and then execute the search.
File organization, and navigation within the file structure, varies from one Android platform to another. Therefore, you may need to try more than one approach when searching for the flow balance report file.
In the eCommission application, in the Air Balancing menu, select Balance report .
In the Balance Report view, in the Device List , select the check boxes to select the MP-V controllers you want to add to the report.
Select Append .
In the eCommission application, on the Air Balancing menu, select Balance report .
In the Balance Report view, select Manage .
In the Balance Report Management view, select the report you want to view or delete.
To delete the report, select Delete .