earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, AS-P
功能: 编程, 安全
产品版本: 2023, 2024
2022/12/17

Adding an Additional SSH Port for an automation Server

If you do not want to connect to your automation server using the SSH port 22, you can add another port.

显示更多
action_close

You can disable port 22 and the USB ports on the automation server.

Port 22

Port 22 is used for communication with Device Administrator. This port is often the target for cyber-attacks. You can disable this port or change the port so that the automation server communicates on another port using SSH. You can also disable all SSH communication.

有关更多信息,请参阅 Disabling Port 22 on an Automation Server .

有关更多信息,请参阅 Adding an Additional SSH Port for an automation Server .

USB port

To prevent anyone from tampering with your automation servers on site you can disable the USB ports.

The USB ports can be disabled on both the AS-B and AS-P servers but not on the automation server AS. The setting is visible on the automation server AS but grayed out and cannot be changed.

有关更多信息,请参阅 Disabling the USB Port on an Automation Server  .

To add an additional SSH port for an automation server
  1. In WorkStation, in the System Tree pane, select the automation server.

  2. Click the Properties tab.

  3. Click the Network tab.

  4. Click Port Settings .

  5. In the Additional SSH port box, select Enable .

  6. In the Additional SSH port number box, enter the port number.

  7. Click Save .

  • Disable Automation Server Ports