Use the SmartX Sensor Touchscreen Display model functions menu to perform a variety of tasks. For example, with the functions menu configured as shown, you can perform the following tasks:
Change occupancy
Change fan speed
Change the degree type
Change heating or cooling mode
Adjust the temperature setpoint
Control the lights
Control the blinds
Configure scenes
Button |
Description |
|
Click to return to the front menu screen. |
|
Click to change the occupancy mode. For more information, see Changing the Occupancy Mode . |
|
Click to access the fan speed menu where you can toggle to the desired fan state. For more information, see Selecting the Fan Speed . |
|
Click to switch the degree type from Fahrenheit to Celsius or Celsius to Fahrenheit. For more information, see Selecting the Degree Type . |
|
Click to access the heating and cooling menu, where you can toggle to the available choices: heating, cooling, or automatic. For more information, see Changing the Heating and Cooling Mode . |
|
Click this button to adjust the temperature setpoint. For more information, see Changing the Temperature Setpoint . |
|
Click this button to turn the lights on or off, or dim the lights. For more information, see Turning the Lights On and Off . For more information, see Dimming the Lights . |
|
Click this button to fully open and close the blinds or incrementally adjust the blinds. For more information, see Fully Opening and Closing the Blinds . For more information, see Incrementally Adjusting the Blinds . |
|
Click this button to access the scenes menu. For more information, see Selecting the Scenes Menu . |