Use the
Device Restart
function of the eCommission SmartX Controllers mobile application to perform a restart of the SmartX IP controller. There are four different ways to restart the SmartX IP controller.
Restart Type
|
Description
|
Warm Start
|
Perform a Warm Start when you want to reset the controller and want to retain all Warm Start properties and Cold Start properties. Perform a Warm Start to troubleshoot any device malfunctions.
|
Cold Start
|
Perform a Cold Start when you want to reset the controller and want to retain all Cold Start properties which excludes Warm Start properties. Perform a Cold Start to troubleshoot any device malfunctions after a Warm Start has not resolved the issue.
|
Erase Controller Database
|
Erase the controller database to clear any applications in the controller and before deploying a new application. Erasing the controller database will retain only the network settings, RSTP, and BACnet ID. As a best practice, erase the controller database before deploying a new application to the controller.
|
Activate IP Changes
|
Select Activate IP Changes when you have made changes to any of the IP settings in order for the changes to take effect.
|
For more information, see Restarting a SmartX IP Controller
.