earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: eCommission SmartX Controllers, IP-IO , MP-C, MP-V, RP-C
Funktionaliteter: Maskinteknik, SmartX IP-kontrollenheter
Produktversion: 3.3
2021-07-23

Restarting a BACnet/IP Controller

Use the Device Restart function to perform a device restart of the BACnet/IP controller.

Visa mer
action_close

Use the Device Restart function of the eCommission SmartX Controllers mobile application to perform a restart of the BACnet/IP controller. There are four different ways to restart the BACnet/IP controller.

Restart Type

Description

Warm Start

Perform a Warm Start when you want to reset the controller and want to retain all Warm Start properties and Cold Start properties. Perform a Warm Start to troubleshoot any device malfunctions.

Cold Start

Perform a Cold Start when you want to reset the controller and want to retain all Cold Start properties which excludes Warm Start properties. Perform a Cold Start to troubleshoot any device malfunctions after a Warm Start has not resolved the issue.

Erase Controller Database

Erase the controller database to clear any applications in the controller and before deploying a new application. Erasing the controller database will retain only the network settings, RSTP, and BACnet ID. As a best practice, erase the controller database before deploying a new application to the controller.

Activate IP Changes

Select Activate IP Changes when you have made changes to any of the IP settings in order for the changes to take effect.

Mer information finns i Restarting a BACnet/IP Controller .

To restart a BACnet/IP controller
  1. In the Device List view, select the BACnet/IP controller you want to restart and select Next .

  2. From the Menu button, select Device Restart .

  3. In the Device Restart page, select the type of restart you want to perform. Mer information finns i Restarting a BACnet/IP Controller .

    Obs!

    You cannot perform a restart with a controller that is hosted.

  4. Select Restart .

  5. A Warning window appears. Select Ok .

The controller is restarted and its functionality is restored.

  • Device Restart
  • Creating a Common Device Settings File