Funktionaliteter: Användarhantering
Produktversion: 2024, 7.0
2025-05-13

Creating Relative Path Templates

You create a relative path template to facilitate the process of assigning path permissions.

Visa mer
action_close

Relative path permissions for a folder structure grant a specific set of permissions to a user account group or to a user account to all the folders accessible in a predefined path and its folder structure. Relative path permissions enable a user accounts group or a user account to reuse a specific path permission.

Furthermore, you can add and delete permissions for this folder structure.

Example

The same set of objects and properties (values, trends, alarms, graphics etc.) is defined in 100 rooms in your building. You define a relative path template that models the folder structure of the rooms in the building, and you define permissions to this folder structure. You define a relative path template by choosing one example of the folder structure. All similar folder structures following the same pattern will inherit permissions defined on the template. Finally, you also define permissions for specific user accounts and user account groups.

Mer information finns i Creating Relative Path Templates .

Relative Path Permissions Rules

You set permissions on a relative path twice.

First, you set permissions on the objects in the template. Objects in the template can be granted the following path permissions: Read, Write, Create, Delete, Edit, Force and Command.

Second, you set permissions for user accounts and user account groups. A user account or a user account group can be granted the following path permissions: Read, Write, Create, Delete, Edit, Force and Command.

Mer information finns i Relative Path Permissions Rules .

To create a relative path template
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Relative path permissions .

  4. In the File menu, click New and then click Relative path permissions .

  5. In the Create Object dialog box, in the Name box, type the name of your path permission.

  6. In the Path box, enter the path.

  7. In the Description box, type a description.

  8. Click Create .

  9. In the System Tree pane, select the relative path permission you just created.

  10. In the  Relative to box, browse to the path you want your permission to be relative to.

  11. Select + .

  12. In the Select Object window, select the object you want to add to the permission path.

  13. In the rules table, choose the permission level for the path.

  14. Click the Save button

     
    action_zoom_plus_stroke
    .

You can assign the created type permissions to user accounts or user account groups.

  • Relative Path Permissions
  • Editing Relative Path Permissions Templates
  • Assigning Relative Path Permissions to User Accounts or User Account Groups