Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Gestión de usuarios
Versión del producto: 2.0, 2.1, 3.0, 3.1
18/05/2018

Removing Path Permissions Templates

You remove path permissions templates to disable all user accounts and user account groups from accessinga specific folder structure.

To remove a path permissions template
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Type permissions .

  4. In the System Tree pane, select the type permissions you want to remove.

  5. In the Edit menu, select Delete .

The template of a path permission is deleted.

  • Type Permissions Rules
  • Software Permissions Rules Management
  • Creating Type Permissions Templates
  • Editing Type Permissions Templates
  • Removing Path Permissions Templates
  • Assigning Type Permissions to User Accounts or User Account Groups
  • Removing Type Permissions from User Accounts or User Account Groups