earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Como

Como


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Gestão de utilizadores
Versão do produto: 3.2, 3.3, 2022
15-10-2020

Removing Type Permissions from User Accounts or User Account Groups

You remove type permissions from a user account or a user account group to withdraw their permissions to a specific type.

Mostrar mais
action_close

You set permissions on a type twice.

First, you set permissions on the type of object. Types can be granted the following path permissions: Read, Write, Create, Delete, Edit, Force, Command and Inherited. You need to assign at least Read permissions on the type.

Second, you set permissions for user accounts and user account groups. A user account or a user account group can be granted or refused permissions to the type.

Tabela: Software Permissions Rules

Property

Description

Read

Permits viewing and listing path content

Write

Permits an administrator to change configurations except for bindings, programs, and graphics

Create

Permits creating new objects on the path

Delete

Permits deleting objects under the path. Delete permissions are required on a folder to delete its contents

Edit

Permits editing objects on the path

Force

Permits forcing values on the path

Command

Permits the execution of commands on the path. Command permissions can override this permission for specific commands

Inherited

Indicates that the permissions are inherited from the parent folder

Nota

You need delete permissions to rename, paste and duplicate folders and objects in EcoStruxure Building Operation software.

Nota

You can always edit graphic and program objects in the relevant editor, however in order to save it on your server you need "Edit" permissions. You can save your edits on your hard drive or export to a location of your choice even if you don’t have “Edit” permissions.

To remove type permissions from a user account or a user account group
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. In the Control Panel tab, in the User Management list, select the user account, or the user account group, you what to assign the type permissions to.

  3. Click Software permissions .

  4. In the Type Permissions pane, select the type permissions you want to remove.

  5. Click the Delete button.

Type permissions are removed from the user account or the user account groups.

  • Type Permissions Rules
  • Software Permissions Rules Management
  • Creating Type Permissions Templates
  • Editing Type Permissions Templates
  • Removing Path Permissions Templates
  • Assigning Type Permissions to User Accounts or User Account Groups
  • Removing Type Permissions from User Accounts or User Account Groups