earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: SpaceLogic Sensors
Functionalities: Hardware
Product version: 2.0, 2.1, 3.0
5/18/2018

SmartX Sensor Models

SmartX Sensors include blank cover and occupancy sensor-only cover models, as well as several models with pushbutton or display-driven user interfaces that allow you to control temperature, occupancy, overrides, and a variety of other settings in a designated living space.

 
action_zoom_plus_stroke SmartX Sensor Models
Figure: SmartX Sensor Models

SmartX Sensor 3-button Cover Model

The 3-Button Cover model contains a passive, infrared sensor for occupancy detection and a plus and minus button to adjust the temperature setpoint. There is also an occupancy override button should the room occupant wish to confirm their presence, turn on the lights, and change the setpoint to a comfortable level.

For more information, see SmartX Sensor 3-Button Cover Model .

SmartX Sensor LCD Temperature Sensor Model

The LCD Temperature Sensor model is the relatively inexpensive, mid-range model with a small LCD display and three buttons to increment (plus), decrement (minus) and then select options (middle button) as you scroll through its menus.

For more information, see SmartX Sensor LCD Temperature Sensor Model .

SmartX Sensor Touchscreen Display Model

The Touchscreen Display model provides a menu-driven interface with a main menu and an optional default or home screen configurable through EcoStruxure Building Operation.

For more information, see SmartX Sensor Touchscreen Display Model .

  • SmartX Sensor Modular Bases and Covers
  • SmartX Sensor 3-Button Cover Model Interface
  • SmartX Sensor LCD Temperature Sensor Model
  • SmartX Sensor Touchscreen Display Model