earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: eCommission SmartX Controllers, IP-IO , MP-C, MP-V, RP-C
Funkcje: Inżynieria, Urządzenia SmartX IP Controller
Wersja produktu: 2022
2025-02-13

Managing Projects in the Controller List Creator

In the Project List view of the Controller List Creator function, you can view existing projects and delete or create new ones.

Pokaż więcej
action_close

The Commission mobile application allows you to use a mobile device to perform commissioning, flow balance, and checkout operations on SpaceLogic BACnet/IP devices. BACnet/IP devices include BACnet/IP controllers (MP and RP), and IP-IO modules. The Commission mobile application is available for Android and iOS (Apple) phones and tablets, as well as devices using Microsoft Windows 10. The Commission mobile application can connect to a single BACnet/IP device or to a network of BACnet/IP devices on the local network.

Device Connection

The Commission mobile application supports device connection through BACnet Wi-Fi and wireless Bluetooth connection.

Więcej informacji zawiera Device Connection .

Bluetooth Adapter

The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to MP controllers. You plug the Bluetooth Adapter into the corresponding SpaceLogic Sensor to connect to the controller.

Więcej informacji zawiera SpaceLogic Bluetooth Adapter .

Device Configuration

You download an image to a BACnet/IP controller to facilitate device commissioning tasks and then use the Device Settings view to configure the settings of the BACnet/IP controller.

Więcej informacji zawiera BACnet/IP Controller Device Settings .

Configuration Menu

Configuration Menus are a group of pre-engineered objects and values that make device commissioning faster and easier. Configuration Menus are exported and downloaded from image files. Download a Configuration Menu to a BACnet/IP controller to commission the controller.

Więcej informacji zawiera Configuration Menu .

I/O Checkout

After you have wired the physical inputs and outputs of the controller, you perform I/O checkout to verify that the wiring was done correctly and that the physical inputs and outputs are working properly.

Więcej informacji zawiera I/O Checkout Overview .

Flow Balancing

The Flow Balance function of the Commission mobile application is used to air balance terminal boxes controlled by MP-V controllers. This function automates most of the air balance procedure but it also allows you to manually check out the flow balance by driving the damper to a specified position, a flow setpoint, or a flow value.

Więcej informacji zawiera Flow Balancing .

Device Restart

Use the Device Restart function of the Commission mobile application to perform a restart of the BACnet/IP controller. There are four different ways to restart the BACnet/IP controller.

Więcej informacji zawiera Device Restart .

To manage projects in the Controller List Creator
  1. In the Controller List Creator , click the File Folder button

     
    action_zoom_plus_stroke
    at the top of the window.

  2. In the Project List view, review the list of existing projects created with the Commission mobile application.

  3. Choose whether to delete a project or create a new one:

  4. When finished, select Continue to return to the List Creator view.

You have reviewed the project list, and deleted projects or created a new one.

  • Commission Mobile Application Overview
  • Capturing a Device with the Controller List Creator