earth_america
user_standard Log on
action_search_stroke
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Commission, IP-IO , MP-C, MP-V
Functionalities: Engineering
Product version: 2.0, 2.1
3/14/2019

Connecting to Single SmartX IP Controller by Wire

Running the eCommission SmartX Controllers mobile application on a Windows laptop computer, you can connect directly to a SmartX IP controller by Ethernet wire. Optionally, you can use an Ethernet switch to connect the computer and the SmartX IP controller.

Show More
action_close

Use this workflow to connect the eCommission SmartX Controllers mobile application to SmartX IP controllers.

Related information can be found in the sections that follow the flowchart.

 
action_zoom_plus_stroke eCommission Application Connection Workflow
Figure: eCommission Application Connection Workflow
Download, install, and activate the eCommission application

Download, install, and activate the eCommission application, and accept the end user license agreement.

For more information, see Downloading and Starting the eCommission SmartX Controllers Mobile Application .

For more information, see Launching and Activating the eCommission SmartX Controllers Mobile Application .

Power up the controllers

Power up the SmartX IP controllers.

For more information, see Powering Up MP-C .

For more information, see Powering Up MP-V .

Prepare a wired or wireless connection for eCommission application

Prepare a wired or wireless connection for use with the eCommission application mobile device.

Connection Type

More Information

Connection Type

More Information

Wired connection to a single controller

For more information, see Connecting to Single SmartX IP Controller by Wire .

Wired connection to a network of controllers

For more information, see Connecting to Network of SmartX IP Controllers by Wire .

Wireless connection to a network of controllers via a WiFi router

For more information, see Connecting to Network of SmartX IP Controllers through WiFi Router .

Wireless connection to a network of controllers via a wireless access point

For more information, see Connecting to Network of SmartX IP Controllers through a Wireless Access Point .

Start the eCommission application and discover controllers

Start the eCommission application and then discover the SmartX IP controllers on the network.

For more information, see Downloading and Starting the eCommission SmartX Controllers Mobile Application .

To connect to a single SmartX IP controller by wire
  1. Configure the network connections on the eCommission application computer and the SmartX IP controller for DHCP addressing.

    For more information, see Configuring SmartX IP Controller Device Settings .

  2. Connect an Ethernet cable between the eCommission application computer and Port 1 of the SmartX IP controller. If you are using an Ethernet switch, connect the computer and the controller to the switch, using Ethernet cables.

    Important:

    Because an actual DHCP server is not used, both the eCommission application computer and the SmartX IP controller will self-assign link-local IP addresses.

  3. In the eCommission application, on the Select Connection view, tap or click the WiFi icon

     
    action_zoom_plus_stroke
    to start Ethernet networking.

  4. In the Device List view, select the SmartX IP controller to make the connection.

    Note:

    The Device List view has filters that allow you to easily find and select the controller:

    • If you are logged in as a Flow Balancer, the device list is automatically filtered to show only MP-V controllers.

    • If you are logged in as a Technician or Electrician, you can sort the list of discovered devices by controller model.

Using the eCommission application, you can now perform tasks on the connected SmartX IP controller as needed.

  • Connection Workflow for the eCommission Application
  • Configuring SmartX IP Controller Device Settings