earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Specifications

Specifications


Products: Project Configuration Tool
Functionalities: Engineering
Product version: 3.2, 3.3, 2022, 2023, 2024, 7.0, 7.1
4/24/2026

Project Configuration Tool – Version 2

arrow1_rotationIntroduction arrow1_rotationFeatures arrow1_rotationSpecifications
 
action_zoom_plus_stroke Project Configuration Tool
Figure: Project Configuration Tool

Introduction

Project Configuration Tool is a powerful software tool that enables you to virtually engineer an EcoStruxure BMS. With this tool, you can reduce the time spent on site by designing, programming, and configuring the EcoStruxure BMS off-site. Project Configuration Tool enables you to run the Enterprise Central, Enterprise Server, and automation servers virtually, and simulate most system functions, before you deploy the servers to the target EcoStruxure BMS.

Features

The Project Configuration Tool sever provides an environment within which all virtual EcoStruxure BMS servers of the project can run while being engineered. Project Configuration Tool provides a web browser based user interface for project management. WorkStation provides a full-featured user interface for configuration of EcoStruxure BMS servers.

Project Configuration Tool is available for Windows and for Linux.

Efficient project management

Using your web browser to access the Project Configuration Tool server, you can easily create projects, create, start, and stop virtual EcoStruxure BMS servers, and deploy the virtual servers to on-site servers. You can also add project properties to keep track of information such as project manager and description.

Virtual EcoStruxure BMS servers

By means of the virtual EcoStruxure BMS servers, you can simulate all aspects of the Enterprise Central, Enterprise Server, and automation servers, except for communication with field devices. Project Configuration Tool for Windows leverages hardware virtualization technology through the Microsoft Hyper-V software. Project Configuration Tool for Linux is running native in the operating system. You can add several virtual EcoStruxure BMS servers to a project at the same time, and you can start and stop the servers to suit your current needs.

Engineering efficiency through templates

Creating virtual automation servers from templates can greatly simplify your engineering efforts and can help improve configuration consistency across projects. With Project Configuration Tool, you can select a backup set for an automation server, save it as a new template, and then create multiple virtual automation servers from that single template. The templates are stored in a library for convenient reuse.

WorkStation for EcoStruxure BMS server configuration
 
action_zoom_plus_stroke WorkStation launched from Project Configuration Tool
Figure: WorkStation launched from Project Configuration Tool

Working with virtual EcoStruxure BMS servers in WorkStation is similar to working with online EcoStruxure BMS servers in WorkStation. The same powerful engineering features and tools are available when you start WorkStation through Project Configuration Tool. Two different color schemes differentiate the products so it is easy to know which tool you are using. With WorkStation, you can create devices, bindings, graphics, alarms, and other objects required for the project. For more information, see the WorkStation Specification Sheet.

Easy project deployment

Using the backup and restore functionality, you deploy the project's virtual EcoStruxure BMS servers to the on-site Enterprise Central, Enterprise Server, and automation servers, to download the configurations that you have created off site. After the deployment, you can log on with WorkStation to an on-site EcoStruxure BMS server to make configuration changes.

Two installation options

Project Configuration Tool can be installed with both internal and external virtual network switches. For local access only, the external switch should be disabled or not configured during installation. This flexibility supports adapting the installation to project-specific requirements. In addition, you have the flexibility to install only the server packages you require. As new versions of EcoStruxure Building Operation are released, you can easily add them to your existing Project Configuration Tool server.

Project Configuration Tool should only be deployed in private isolated networks and should not be exposed directly to the Internet.

EcoStruxure Building Operation software compatibility

Project Configuration Tool supports EcoStruxure Building Operation version 3.2 and later. These server packages support creating and running virtual servers and engineering projects.

Project Configuration Tool also supports upgrading from EcoStruxure Building Operation version 1.9, 2.0, 3.0, and 3.1 to version 7.0.2 or later. These legacy server packages are provided solely for upgrade purposes and are not intended to run as active servers.

Upgrade capability

Project Configuration Tool enables you to upgrade EcoStruxure BMS servers to supported EcoStruxure Building Operation versions by running the upgrade workflow on existing virtual servers or by importing project backups into the virtual environment and applying the same process. This applies to EcoStruxure Building Operation version 3.2 and later server packages, allowing you to prepare and test upgrades off-site using the virtual servers in Project Configuration Tool.

One-step upgrade from EcoStruxure Building Operation versions 1.9–3.1

Project Configuration Tool provides a one-step upgrade path for EcoStruxure BMSs based on EcoStruxure Building Operation versions 1.9, 2.0, 3.0, and 3.1. These special legacy server packages are provided specifically for importing older system backups and upgrading them directly to EcoStruxure Building Operation version 7.0.2 or later in a single workflow. These packages are not intended to run as active servers inside Project Configuration Tool and exist solely to support this upgrade process. This unified, one-step workflow enables upgrades for both existing Project Configuration Tool projects and imported legacy systems.

Specifications

Hardware requirements – Server
Processor power, memory, and storage capacity should be scaled upwards to accommodate targeted system size as impacted by the total quantity of EcoStruxure BMS projects. Project Configuration Tool is tested on a server with an 8-core 3.6 GHz processor, 32 GB of memory, and storage capacity of 1 TB.
Installing Project Configuration Tool and the virtual machine require approximately 50 GB of storage space on the installation drive. Project Configuration Tool for Windows also requires 5 GB on the Windows Temp folder, which is typically located on the C drive (C:).
Processor
Minimum: Intel Core i7 7820X @ 3.6 GHz, or another x86-64 processor with comparable performance (minimum 4 CPU cores)
  
Recommended: Intel Core i7 class processor @ 4.0 GHz or better, with 6 or more CPU cores
Memory
2 GB plus 170 MB x number of running EcoStruxure BMS servers
  
Minimum: 16 GB
  
The Virtual Machine is configured by default with 8 GB.
Storage capacity - Project Configuration Tool for Windows
Minimum: 50 GB and 5 GB in Windows Temp folder
  
Recommended: 1 TB or higher
Storage capacity - Project Configuration Tool for Linux
Minimum: 50 GB
  
Recommended: 1 TB or higher
BIOS
Required BIOS configuration
Intel VT-x or AMD-V virtualization support enabled
Memory and processor capacity
The memory capacity is a function of the number of running servers, devices, and objects in the projects. The memory consumption is approximately 2 GB plus 170 MB x number of running servers. The Virtual Machine is configured by default with 8 GB, which can be changed in Hyper-V. With 4 CPU cores, it is typically possible to run up to 100 servers. To run 100 to 200 servers, the requirement is 8 CPU cores. To run 200 to 250 servers, the requirement is 12 CPU cores. The maximum supported number of running servers is 250. The following guidelines are offered to assist in determining the appropriate size:
One empty EcoStruxure BMS server
50 MB
One typical EcoStruxure BMS server
170 MB
One empty b3920
0.07 MB
One empty MNB 1000
0.01 MB
One Xenta 122 FC
1.5 MB
One empty Programmable Xenta
0.04 MB
One MNLRF1_FanCoil
0.36 MB
Disk capacity
Maximum virtual hard disk size - Project Configuration Tool for Windows
200 GB
The disk space used depends on the types of configurations. The following guidelines can be used to determine approximately how much disk space will be used:
One empty EcoStruxure BMS server
100 MB
One typical automation server
250 MB
One typical Enterprise Server
500 to 2000 MB
100 input/outout points
0.5 MB
100 trend logs or alarms
0.3 MB
Graphic
1 to 100 MB
Program
0.1 to 10 MB
10 empty MP-C controllers
1 MB
10 empty Modbus devices
0.5 MB
100k events
25 MB
Creating backup
Server size + 100 MB
Software requirements
Operating systems – Project Configuration Tool for Windows
Microsoft Windows 11
  
Microsoft Windows Server 2019
  
Microsoft Windows Server 2022
  
Microsoft Windows Server 2025
The following Microsoft Windows 11 editions are supported: Pro and Enterprise.
The following Microsoft Windows Server 2019 editions are supported: Datacenter, Standard, and Essentials.
The following Microsoft Windows Server 2022 editions are supported: Datacenter, Standard, and Essentials.
The following Microsoft Windows Server 2025 editions are supported: Datacenter, Standard, and Essentials.
Operating systems – Project Configuration Tool for Linux
Ubuntu 22.04 LTS, Desktop and Server
  
Ubuntu 24.04 LTS, Desktop and Server
Hyper-V - Project Configuration Tool for Windows
Hyper-V must be enabled
Required additional software - Project Configuration Tool for Windows
Microsoft .NET Framework 4.7.2 and later
  
WorkStation version 5.0.3.5001 and later a
Compatibility
Runtime compatibility
EcoStruxure Building Operation server packages
version 3.2 and later
WorkStation
version 3.2.4, 4.0.5, 5.0.3, and later
Upgrade-only compatibility
EcoStruxure Building Operation server packages a
version 1.9, 2.0, 3.0, and 3.1
Communication between Project Configuration Tool server and web browser or WorkStation
HTTPS
Non-binary, port not configurable, default 443
Part numbers
No part number or license for Project Configuration Tool. However, WorkStation used for EcoStruxure BMS server configuration requires a WorkStation license. For more information, see the WorkStation Specification Sheet.