The RP-C comes in four different models, which offer four different sets of I/O point types, named 12A, 12B, 12C, and 16A.
The RP-C-12A, -12B, and -12C models support 24 VAC/DC input power, whereas the RP-C-16A model supports 230 VAC input power.
Model |
I/O Set |
Input Power |
RP-C-12A-F-24V |
12A |
24 VAC at 50/60 Hz or 24 to 30 VDC |
RP-C-12B-F-24V |
12B |
24 VAC at 50/60 Hz or 24 to 30 VDC |
RP-C-12C-F-24V |
12C |
24 VAC at 50/60 Hz or 24 to 30 VDC |
RP-C-16A-F-230V |
16A |
230 VAC at 50/60 Hz |
Para obtener más información, consulte RP-C Onboard I/O .
Para obtener más información, consulte RP-C Built-in Power Supply .
All RP-C models have the same small footprint.