earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: RP-C
功能: 硬件
产品版本: 3.0, 3.1
2023/12/12

RP-C LEDs

arrow1_rotationStatus LED

There is one LED on the front panel of the RP-C.

 
action_zoom_plus_stroke RP-C LEDs
图: RP-C LEDs

表格: RP-C LEDs

Function

Color

Status

Red, Green, Blue (and combinations)

Status LED

The RP-C Status LED indicates the condition of the device.

表格: RP-C Status LED Patterns

LED Patterns

Condition

Green, constant

Normal operation, status OK

RP-C controller firmware application running

Green, flashing (~1 Hz)

Device restarting, wait

RP-C controller firmware application running

Red, constant

Detected error, attention required

Red, flashing (~1 Hz)

Device operates, but a problem needs attention

Red/green, flashing (~1 Hz)

RP-C I/O board receiving software upgrade, wait

Do not interrupt power to the controller. For more information, see the following Important note.

Amber, constant

RP-C controller firmware boot applet running

Amber, flash

Device restarting, wait

RP-C controller firmware boot applet started

Amber/green, flashing (~1 Hz)

RP-C controller firmware is being upgraded. It is typically the firmware main application, but it can also be a boot applet.

White, transient

Device starting, wait

White, constant

RP-C controller firmware not running, attention required (contact product support)

重要:

Avoid power interruptions to the device during the brief period when the Status LED is flashing red and green. An interruption causes problems with the I/O processor upgrade and can result in corrupt firmware. You can view the evidence of a corrupt processor when the device reports itself as an “MP-C-15A.” A corrupt I/O processor can lead to the loss of the reset button and/or I/O functionality, as well as the inability to upgrade the I/O processor and/or the device.

  • RP-Cs
  • Status LEDs