The Status LED on the front of the SmartX devices changes color and flashes to indicate the status of the device.
The remaining LEDs on the front differ in number and meaning for the different devices and are explained in the sections about the specific device.
The SmartX server Status LED indicates the condition of the device.
LED Patterns |
Condition |
Green, constant |
Normal operation, status OK |
Green, flashing (~1 Hz) |
Device restarting, wait |
Green, flashing (~10 Hz) |
Device shutting down |
Red, constant |
Detected error, attention required |
Red, flashing (~1 Hz) |
Device operates, but a problem needs attention |
Red/green, flashing (~1 Hz) |
Device firmware upgrade (DFU) mode or firmware being downloaded in DFU mode |
No light |
No input power |
The I/O module Status LED indicates the condition of the device.
LED Patterns |
Condition |
Green, constant |
Online and configured (at least one channel/point downloaded successfully) |
Green, constant Red, flashing (for 100 ms every 2 s) |
Online and configured Disabled Hand-Off-Auto (HOA) override switches Applies only to I/O modules with HOA override switches and with manufacturing date earlier than 2021-W26 and upgraded with firmware version 2.017 or later. 有关更多信息,请参阅 Important Information on Central IO Modules with Manufacturing Date Earlier Than 2021-W26 . |
Green, flashing (200 ms ON, 200 ms OFF) |
Online and unconfigured (physical module that either matches/mismatches logical module) |
Green, slow flashing (approximately every 3 s) |
Low power mode (saves energy) |
Red, constant |
Error requiring attention (for example, the input voltage is too low) |
Red, flashing (100 ms ON, 100 ms OFF) |
Offline with respect to the SmartX server (both configured and unconfigured modules) |
Red/Green, flashing (green 100 ms, red 100 ms) |
Bootloader mode (downloading data) |
No light |
No input power |
The PS-24V power supply Status LED indicates the condition of the device.
LED Patterns |
Condition |
Green, constant |
Output voltage and load OK |
Red/green, flashing |
Output slightly overloaded |
Red, constant |
Output overloaded |
No light |
No input power |
The MP Series controller Status LED indicates the condition of the device.
LED Patterns |
Condition |
Green, constant |
Normal operation, status OK MP Series controller firmware application running |
Green, flashing (~1 Hz) |
Device restarting, wait MP Series controller firmware application running |
Red, constant |
Detected error, attention required |
Red, flashing (~1 Hz) |
Device operates, but a problem needs attention |
Red/green, flashing (~1 Hz) |
MP Series controller I/O board receiving software upgrade, wait Do not interrupt power to the controller. For more information, see the following Important note. |
Amber, constant |
MP Series controller firmware boot applet running |
Amber, flash |
Device restarting, wait MP Series controller firmware boot applet started |
Amber/green, flashing (~1 Hz) |
MP Series controller firmware is being upgraded. It is typically the firmware main application, but it can also be a boot applet. |
The IP-IO module Status LED indicates the condition of the device.
LED Patterns |
Condition |
Green, constant |
Normal operation, status OK IP-IO module firmware application running |
Green, flashing (~1 Hz) |
Device restarting, wait IP-IO module firmware application running |
Red, constant |
Detected error, attention required |
Red, flashing (~1 Hz) |
Device operates, but a problem needs attention |
Red/green, flashing (~1 Hz) |
IP-IO module I/O board receiving software upgrade, wait Do not interrupt power to the I/O module. For more information, see the following Important note. |
Amber, constant |
IP-IO module firmware boot applet running |
Amber, flash |
Device restarting, wait IP-IO module firmware boot applet started |
Amber/green, flashing (~1 Hz) |
IP-IO module firmware is being upgraded. It is typically the firmware main application, but it can also be a boot applet. |
The RP-C Status LED indicates the condition of the device.
LED Patterns |
Condition |
Green, constant |
Normal operation, status OK RP-C controller firmware application running |
Green, flashing (~1 Hz) |
Device restarting, wait RP-C controller firmware application running |
Red, constant |
Detected error, attention required |
Red, flashing (~1 Hz) |
Device operates, but a problem needs attention |
Red/green, flashing (~1 Hz) |
RP-C I/O board receiving software upgrade, wait Do not interrupt power to the controller. For more information, see the following Important note. |
Amber, constant |
RP-C controller firmware boot applet running |
Amber, flash |
Device restarting, wait RP-C controller firmware boot applet started |
Amber/green, flashing (~1 Hz) |
RP-C controller firmware is being upgraded. It is typically the firmware main application, but it can also be a boot applet. |
White, transient |
Device starting, wait |
White, constant |
RP-C controller firmware not running, attention required (contact product support) |