AD v3 Communication and Power
AD v3 uses a wired (USB) connection to communicate with SmartX servers and the device must be powered by a 24 VDC power supply.
AD v3 has a screw hole on the back cover and the device is delivered with a screw and a washer (M4 x 10 mm Phillips pan head machine screw with external tooth washer) for connection of an earth ground wire.
Communication over a Wired (USB) Connection
The preinstalled USBnet driver enables AD v3 to communicate with SmartX servers over a wired (USB) connection.
24 VDC power supply
AD v3 must be powered by a 24 VDC power supply. The Y-shaped cable (SXWADUSBC10002 or SXWADUSBC10003) enables data communication and power supply over a single cable. Only cables designed for AD v3 must be used. The required cables can be ordered from Schneider Electric.
Aviso
|
USB DEVICE DAMAGE
Do not use the Y-shaped cable to power any USB devices other than AD v3.
Failure to follow these instructions can result in USB device damage.
|
Aviso
|
LOSS OF DATA OR POWER
Use only cables ordered from Schneider Electric.
Use only cables that are designed for AD v3.
Do not use cables that exceed 3 m (10 ft).
Failure to follow these instructions can result in loss of data or power.
|
action_zoom_plus_stroke
Figura:
Wired (USB) connection to a SmartX server and power from a 24 VDC power supply
Hardware Overview
AD v3
Installing AD v3 on a Cabinet
Connecting AD v3 to a SmartX Server and a 24 VDC Power Supply