earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Dashboards
Product version: 3.0, 3.1, 3.2, 3.3, 2022, 2023
2/23/2024

Log Gauge Properties Dialog Box

Use the Log Gauge Properties dialog box to configure and edit a log gauge.

 
action_zoom_plus_stroke Log Gauge properties – dialog box
Figure: Log Gauge properties – dialog box

Table: Log Gauge Properties – Dialog Box

Component

Description

Display trend log

Enter the trend log you want to display.

Period

Select the period you want to display.

Calculation method

Select the calculation method for the trend log. For more information, see Calculation Methods .

Caption

Type a caption for the widget.

Caption Link

Select to make a link to an object that is relevant to the values that are displayed in the widget.

Min

Enter the minimum value for the gauge.

Max

Enter the maximum value for the gauge.

Guides

Use the guides to define the colors for different values and value ranges.

For more information, see Log Gauge .

Add

Click to add a guide to define the colors for different values and value ranges.

For more information, see Log Gauge .

Value

Select a value for the guide in the widget.

Color

Select a color for the value for the guide in the widget.

Description

Type a description.

Indicator color

Select the indicator color for the needle or the indicator in the gauge.

For more information, see Log Gauge .

Decimals

Select the number of decimals you want to display.

Show Period

Select to display the period as a legend.

Use needle

Select True to use a needle as indicator in the gauge. If no needle is selected the gauge displays the value as an indicator instead.

  • Dashboard Widgets
  • Log Gauge
  • Widget Dialog Box – Layout Tab