earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: WebStation
Funkcje: Dashboards
Wersja produktu: 3.0, 3.1, 3.2, 3.3, 2022, 2023
2024-02-23

Point Gauge

A point gauge is used to graphically display a current value in a gauge.

Using the guides, you can configure the scale of the gauge to display different colors in different ranges on the scale.

You can use two methods to display the value in the gauge: a needle or an indication scale inside the gauge.

For example, you want a log gauge that displays log values between 0 and 30. Values between 10 and 20 are ok and will be marked green. Values between 20 and 30 are too high and will be marked red. You want a needle to indicate the value on the gauge scale.

You want the log gauge to present values between 0 and 30.

Configure the scale for the gauge using the min value 0 and the max value 30.

Add three Guides in the Guide field and configure them as follows:

  • Value = 10 and color blue. This makes the value range 0 to 10 blue in the gauge.

  • Value = 20 and color green. This makes the value range 11 to 20 green in the gauge.

  • Value = 30 and color red. This makes the value range 21 to 30 red in the gauge.

You can make the indicator color black and use the needle to display the value.

If you do not select Use needle you get a black indicator inside the gauge that displays the value.

  • How Dashboards Work
  • Dashboard Widgets
  • Point Gauge