earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Dashboards
Product version: 3.0, 3.1, 3.2, 3.3, 2022, 2023
2/23/2024

Point Pie Properties Dialog Box

Use the Point pie properties dialog box to to configure and edit a a point pie.

 
action_zoom_plus_stroke Point pie properties dialog box
Figure: Point pie properties dialog box

Table: Point Pie Properties Dialog Box

Component

Description

Add

Click to add a point.

Display variable

Enter the variable you want to display.

Color

Select the color for the variable.

Caption

Type a caption for the widget.

Caption Link

Select to make a link to an object that is relevant to the values that are displayed in the widget.

Pie Center

Select how you want to display the pie center.

For more information, see Point Pie .

Show Legend

Click True to display the name and color of the trend log in the widget.

Show Percentages

Select to display the values in percentage.

Display Values

Select to to display the numerical values.

  • Dashboard Widgets
  • Point Pie
  • Widget Dialog Box – Layout Tab