earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WebStation
功能: Dashboards
产品版本: 2024, 7.0
2024/12/3

Configuring a Log Pie

You configure a log pie to get a graphical presentation of trend logs in a pie chart.

显示更多
action_close

A log pie chart is a circular graphic divided into slices to illustrate proportions of trend logs.

The Log pie can contain one or many logs. The colors and calculation method of every log can be changed.

Pie Center

The pie center can be used to display the following values:

  • None: Does not display any pie chart center.

  • Average: Displays the average value for all logs added to the pie chart.

  • Total: Displays the sum of all logs added to the pie chart.

  • Min: Displays the value of the log with the lowest value.

  • Max: Displays the value of the log with the highest value.

Numerical values

You can get a numerical display of all values in the log pie using the Display Values feature.

To configure a log pie
  1. Click Configure or click the Settings button

     
    action_zoom_plus_stroke
    .

  2. Click Add .

  3. Select the trend logs and click Select .

  4. In the Calculation method box, select a calculation method.

  5. In the Color box, select a color for the trend log.

  6. In the Period box, select a period.

  7. In the Caption box, type a caption.

  8. In the Caption Link box, enter a link to an object that is relevant for the log pie.

  9. In the Pie Center , select a pie center.

  10. In the Show Legend box, select True to display the name and color of the trend log in the log pie.

  11. In the Show Percentage box, select True to display the values in percentage.

  12. In the Show Period box, select True to display the period as a legend.

  13. In the Display Values box, select True to display the numerical values.

  14. Click OK .

  • How Dashboards Work
  • 仪表板小部件
  • Log Pie
  • Log Pie Properties Dialog Box
  • Adding a Widget to a Dashboard