earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: WebStation
Funktionaliteter: Dashboards, Grafik
Produktversion: 3.0, 3.1, 3.2, 3.3, 2022, 2023
2024-02-23

Graphics in Dashboards

Graphics can be added to a dashboard.

When you add a graphic to a dashboard, the graphic keeps all of its functions. For example, links in the graphics to other objects work and values in the graphics can be changed and forced.

The graphics that are already in the Select Dashboard Widgets dialog box are custom types. They are visible in the Custom Types Library in WorkStation. When you add a graphic already in the Select Dashboard Widgets dialog box the graphic is an instance of the custom type.

  • How Dashboards Work
  • Dashboard Widgets
  • Custom Types Overview
  • Custom Types
  • Instances of Custom Types
  • Dashboard Widgets